11/30/2019 2:35 AM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2685) |
Translation from the Spanish text:
Hola jrsoto; Este foro de Siemens atrae participantes de muchos países donde no se habla español. Para facilitar los intercambios hemos escogido Inglés como idioma común. Haznos el favor de escribirnos en inglés a su próxima visita. The Siemens forum attracts participants from many countries where Spanish is not the first tongue. To make exchanges easier between us we have chosen English as an interchange language. Please write to us in English on your next visit. There are no integrated functions in the S7-300 instruction list that allow it to use the Profinet port as a Modbus TCP client or server. But you can purchase an Open Modbus TCP driver either for a CPU with Profinet port or for a CP 343-1 Ethernet processor. These are described in the following FAQ: https://support.industry.siemens.com/cs/us/en/view/22660304 You can also download demo versions of the software, that will allow Modbus TCP exchanges without limit; the drawback is that under demo the fault LEDs on the CPU will remain active and the diagnostic buffer will fill up with alarm messages until you license the driver correctly. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/30/2019 02:39:21Last edited by: dchartier at: 12/01/2019 00:37:30 |
|
Follow us on