11/28/2019 7:41 PM | |
Posts: 1 Rating: (0) |
Hello Dears, I have a simatic OP3 HMI and unfortunately I forget the HMI password. could someone help me how to reset the password? thanks a lot: Gyorgy. |
12/3/2019 8:56 AM | |
Joined: 9/9/2014 Last visit: 7/11/2024 Posts: 246 Rating: (40) |
Hello, Reset a Siemens OP3 panel for reprogram If you have a project from the panel, then it is better to reset everything - set the password again. *********** Default password is 100 Rihgt+Down+Esc= Hold and switchON = Delete Configuration & Set Password Default (100) *********** You can try to test (Hardware test) the panel - then a reset will be performed (the project will be deleted from the panel) - and the project will have to be reloaded (but if there is one)))) Or try using the default password (if it still works) I don’t know other ways to reset the password (maybe someone else will tell) ... |
Best Regards |
|
Follow us on