12/3/2019 10:45 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please check where from main set point signal comes? i.e. 18.3/901 & 18.3/902. When motor & drive running, check, this set point signal, r01 on PMU, r02 on PMU, r019 on PMU values & record those. Also check tacho feed back voltage & note down the same & share all those values here. BTW, is it same machine on which you are also facing NCU problem posted here? Error 2000 plc sign of life monitoring |
This contribution was helpful to1 thankful Users |
12/6/2019 7:02 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Did you got this problem solved? Is the same machine, (refer my earlier post)? |
12/6/2019 8:08 AM | |
Posts: 95 Rating: (0) |
|
12/6/2019 8:09 AM | |
Posts: 95 Rating: (0) |
no sir |
12/6/2019 9:51 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, With same setting, check r023, r025 & r026 values on PMU & report here. |
12/6/2019 10:23 AM | |
Posts: 95 Rating: (0) |
|
Follow us on