7/29/2016 9:39 AM | |
Joined: 4/24/2006 Last visit: 4/19/2024 Posts: 8610 Rating: (1147)
|
Hello, Please have a look at the following link: When you use STEP 7 v5.5, you need a GSD file. And with TIA Portal: Which version are you using at this moment? (Incl. SP and Upd.) Are you using the latest Hardware Support Package? Support Packages for the hardware catalog in the TIA Portal (HSP) Best regards, Wizard |
7/29/2016 9:53 AM | |
Joined: 5/22/2015 Last visit: 4/11/2024 Posts: 118 Rating: (2) |
In the download link of the GSD file I have not found the reference "6ES7155-6BA00-0CN0" :/
|
7/29/2016 11:14 AM | |
Joined: 5/22/2015 Last visit: 4/11/2024 Posts: 118 Rating: (2) |
Yes I have already found |
12/4/2019 10:55 AM | |
Posts: 1 Rating: (0) |
Como la pudiste encontrar en el Step 7 v5.6??? No encuentro el 6ES7155-6BA00-0CN0. |
Follow us on