12/4/2019 3:46 PM | |
Joined: 10/1/2018 Last visit: 7/10/2022 Posts: 66 Rating: (0) |
Hello. I am trying to create a UDF and the following message appears: "Insufficient resources to paste the blocks". *** 12/4/19 5:22 PM КОУ.lsc Attachmentudf error.zip (54 Downloads) |
12/4/2019 4:35 PM | |
Joined: 12/18/2014 Last visit: 4/20/2024 Posts: 32848 Rating: (4061)
|
In German speaking part of the forum found I a topic to this problem. In a reply can you read this....
Edit: In your case I would start a Support Request. |
Last edited by: ixo65 at: 12/04/2019 16:37:11 |
|
This contribution was helpful to1 thankful Users |
12/4/2019 5:41 PM | |
Joined: 12/18/2014 Last visit: 4/20/2024 Posts: 32848 Rating: (4061)
|
It looks like the problem is the LSC version. I have now made a test with LSC V8.2.1and a UDF containing 8 blocks, inserted into an empty diagram and copied 49 times. As a result, all 400 function blocks are used, there was no message because of too high a block number (see "Untitled" in attachment). Only when I wanted to insert another UDF copy, there was an error message. Understandable, because all function block numbers were occupied (see "Untitled_2" in attachment). AttachmentScreenshots.zip (57 Downloads) |
Follow us on