12/5/2019 6:47 AM | |
Joined: 9/9/2014 Last visit: 7/11/2024 Posts: 246 Rating: (40) |
Hello, If you read our forum, opinions differ - on this topic. However, I saw my colleagues test the software redundancy of the S7-300 controllers. Check out the topic below: Possible to test H/R redundancy with S7 simulation Software. and read FAQ: How do you simulate communication between two CPU modules? I am sure (True, I did not check it personally) that this can be done, the main thing is to configure everything correctly Try to do everything as in the example, and then test the redundancy) |
Last edited by: Unreality at: 12/05/2019 06:49:45Last edited by: Jen_Moderator at: 12/05/2019 08:57:53Optimized link. Best Regards |
|
Follow us on