12/1/2019 9:34 PM | |
Joined: 4/3/2019 Last visit: 3/4/2024 Posts: 8 Rating: (0) |
Note: I attach the TIA Portal file with the PLC and Multicontrol controller configured.
AttachmentInterroll.zip (731 Downloads) |
12/5/2019 5:49 PM | |
Joined: 4/3/2019 Last visit: 3/4/2024 Posts: 8 Rating: (0) |
Hi, Thank you for the information. I moved forwards with the project and the problem now is that I am using and Divert rollers and I am using an interface box for that. I send the order for speed and every thing ok but I send the order for rotation and nothing happen. What I did is connect the controller as a "IO device" with PROFINET so I can program it from my PLC. I saw the addresses of the interroll controller and mapped them following the INTERROLL manual. Someone knows if I am doing something wrong with the plc program?. I used a 127 command as well. Note: I attached the TIA Portal file if someone wanted to check. Thank you, Best regards, Alvaro Attachment20191128 Interroll Multicontrol_20191205_1645.zip (530 Downloads) |
Follow us on