12/8/2019 5:40 PM | |
Joined: 6/17/2014 Last visit: 3/30/2024 Posts: 11 Rating: (0) |
This is came with one machine from UK |
12/8/2019 7:55 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: Successor product: 6ES7313-6CG04-0AB0 SIMATIC S7-300, CPU 313C-2 DP Compact CPU with MPI, 16 DI/16 DO, 3 high-speed counters (30 kHz), integrated DP interface, Integr. power supply 24 V DC, work memory 128 KB, Front connector (1x 40-pole) and Micro Memory Card required. Remark: Replacing the CPU with direct successor: do not require to modify in the hardware configuration and you can insert the old MMC in the successor CPU directly. Communications processor CP 343-1 Lean for connection of SIMATIC S7-300 to Industrial Ethernet via TCP/IP and UDP, Multicast, SEND/RECEIVE with and without RFC1006, Fetch/ Write, S7 communication (server), PROFINET IO device integrated 2-port switch ERTEC 200, Module replacement without PG, SNMP diagnostics, initialization via LAN, 2x RJ45 connection for LAN with 10/100 Mbit/s 3-I think every thing is correct except:
Have a look at the following FAQ: How can you set up the online connection again between the PG and the CPU? In some cases it can happen that an online connection cannot be set up between the PG and the module and an error message is displayed. Most causes can be determined through the notes in the Online Help which you reach by clicking on "Help". |
Last edited by: Online Tech at: 12/09/2019 09:47:55Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on