12/10/2019 7:31 AM | |
Joined: 7/22/2019 Last visit: 12/16/2022 Posts: 4 Rating: (1) |
Hello everyone! Did someone find a solution for this problem? I am also in a similar situation : no Profinet communication between PLC and robot. -robot Fanuc R-30iB -CP1604 v2.6, A05B-2600-J930 v8.23 mainboard A05B-2600-C001 -GSDML: GSDML-V2.31-FANUC-A05B2600J930V823D4-20160119.xml installed -PLC : S7-300 319F-3 PN/DP v3.2 -switch: SCALANCE X208 v4.5, 8 ports. The PING command to the IP of the robot works ,but the robot show up as offline in the online hardware config page. I am using Simatic Manager Step 7 V5.5 + SP4. Any thoughts on this? ------------------------------------------------------------------------------------------ |
Last edited by: marian_bica at: 12/10/2019 07:40:18Last edited by: Jen_Moderator at: 12/11/2019 08:31:42New subject after splitting |
|
12/11/2019 8:38 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981)
|
Hello, can you try to connect the robot directly to the PLC, is it then working? Christoph |
Follow us on