12/10/2019 10:33 AM | |
Joined: 3/5/2017 Last visit: 9/13/2024 Posts: 775 Rating: (127) |
HI, Is your report csv file also empty or just report? First make sure you get csv file and then start to work on pdf. And don't use time range on pdf, before you are sure that it gets generated correctly. I attached my settings to get report. It might be missing something, i had to make it in a hurry. And it just just demo which a did to show principle of logging that alarm. No loops or data from plc. My start logging and stop logging buttons are like yours so that part should work. AttachmentAlarmLogging.pdf (504 Downloads) |
Last edited by: K_Ohjus at: 12/10/2019 10:35:05- Trying is the first step towards failure. |
|
12/10/2019 3:16 PM | |
Joined: 3/5/2017 Last visit: 9/13/2024 Posts: 775 Rating: (127) |
Hi, Printing from plc array works fine, well why it should not. Just tested, i had never tried before. I build my reports little different. When you create pdf:s you should use USB instead of SD, it considerably faster. I attached very simple print out of printing an whole array from plc. AttachmentWinCC_Output_10_12_2019_16_56_09.pdf (537 Downloads) |
Last edited by: K_Ohjus at: 12/10/2019 15:20:31- Trying is the first step towards failure. |
|
Follow us on