12/10/2019 8:41 AM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi AMI88, First question: Do you have Process Tag Types which you want to convert to Control Module Types? or do you want to create new Control Module Types? When creating a CMT from PTT, the CMT will be flat out, meaning all IO signals/parameters are listed under the CMT object. However, this is not according to your print screen. In there you created subordinate control modules like Interlock/Permit etc. blocks. When you want this, you must drag en drop the desired blocks in the chart to the Technological IO editor, and than the reference is saved. |
If I could help you, you can use the RATE button. Thank you. |
|
12/10/2019 1:01 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, No problem! So, your question answered? Using subordinate CM is not necessary in a CMT, so I guess developers didn't create the logic for it..but I could be wrong.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
12/10/2019 1:55 PM | |
Joined: 6/13/2016 Last visit: 7/23/2024 Posts: 17 Rating: (1) |
Yeah, now it is clear. Thank you |
Follow us on