12/11/2019 11:14 AM | |
Joined: 12/16/2012 Last visit: 9/13/2024 Posts: 653 Rating: (130) |
Hi! I would like to disagree on that and recommend #1, Tia-Pro1. https://www.sitrain-learning.siemens.com/DE/en/search/index.do There are also e-courses on Sitrain: https://www.sitrain-learning.siemens.com/ELEARNING/en/rw89954/PLCs-for-beginners |
12/11/2019 11:25 AM | |
Joined: 10/25/2019 Last visit: 5/20/2024 Posts: 278 Rating: (20) |
No, let him first just to grope PLC and other related stuff. Programming a bit later. after training courses, consider purchasing of this stuff 6ES7511-1CK02-4YB5. Spend days and nights with this kit. You'll see difference over some time. Otherwise, no success. BR |
This contribution was helpful to1 thankful Users |
12/11/2019 12:43 PM | |
Joined: 12/16/2012 Last visit: 9/13/2024 Posts: 653 Rating: (130) |
Hi! Let me to still disagree with you. First of all you recommend the ST-Serv courses, which are based on the S7-300/400 family and the calssic S7 software together with a training kit based on the new S7-1500 PLC programmed with TIA Portal. So I would definitely recommend a TIA course and based on the target group hendabdelaziz can decide which one is more appropriate: Target Group Programmers Commissioning engineers Engineering personnel Target Group Maintenance personnel Service personnel Operators |
12/11/2019 3:54 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello HBCM_; Opinions will differ on what can be learned at a formal training from Siemens, depending on expectations and amount of participation.I have attended a few training sessions myself, a long time ago, on S7-300 PLCs programming, on WinCC (v3.0!) and on PCS 7. What I retained most was the result of discussions with the teacher during lab periods where we analysed my misunderstandings and the trainer allowed me time to find my own answers, to my satisfaction. Meanwhile, if you do not like the formal training cost, time constraints and environment, you may prefer these free-downloadable tutorials prepared for academic students on the S7-1200 and S7-1500 (TIA Portal basic), from Siemens SCE, so you can develop your expertise on your own time: The attachment below shows the TIA Portal training modules, and the format and languages these modules are available in. If you decide to try that route, I would recommend a S7-1200 starter kit to give you lower-cost equipment bundles to play with and assimilate the tutorial principles and examples, such as these: https://c4b.gss.siemens.com/resources/images/articles/dffa-b10228-00-7600.pdf Daniel Chartier |
Follow us on