1/5/2019 3:50 PM | |
Joined: 1/1/2017 Last visit: 4/22/2024 Posts: 329 Rating: (11) |
Hello, I'm having difficulties in wiring of the following items: 1.6GK19011BB102AB0: Profinet Connector 2.6XV18782A: Industrial Ethernet FastConnect TP standard cable 3.6GK19010DB306AA0: IE FC M12 PLUG PRO 4X2 The problem is that the Cable has 08 no of cores & the Profinet connector has 04 core connection capabilities. Hence that's why I'm facing difficulties in going with the wiring. Waiting for your prompt responses. Regards OmKris |
1/5/2019 4:59 PM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello OMKRIS; This document was provided during a Profinet training, a few years ago. It contains a figure showing the Profinet connector specifications, Figure 8.1: Signal Function Wire colors RJ45 contact assignment TD+ Transmit Data+ Yellow 1 TD- Transmit Data- Orange 2 RD+ Receive Data+ White 3 RD- Receive Data- Blue 6 Hope this helps, Daniel Chartier AttachmentPN-Cabling-Guide_2252_V200_May07.pdf (2949 Downloads) |
This contribution was helpful to6 thankful Users |
1/6/2019 1:30 AM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello Omkris; Standard Profinet cable, as any 100 MBps Ethernet cable, is described as a 2x2 cable, with 4 wires; Your 4-pair (4x2) Ethernet cable is designed for 1GBps Ethernet. https://www.iplocation.net/rj45-wiring Although there are 4 pairs of wires, 10BaseT/100BaseT Ethernet uses only 2 pairs:OrangeandGreen. The other two colors (blueandbrown) may be used for a second Ethernet line or for phone connections.The two wiring standards are used to create a cross-over cable (T-568A on one end, and T-568B on the other end), or a straight-through cable (T-568B or T-568A on both ends). When you are connecting a 4x2 cable in a Profinet connector, you must only use 2 pair, the Orange/White-Orange and the Green/White-Green. The pinout in the connector should be: - Pin 1:White-Orange -Pin 2: Orange - Pin 3: White-Green - Pin 6: Green If the other pairs are nor required for your project, you an discard them at the connector. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/7/2019 3:59:15 PM |
|
This contribution was helpful to3 thankful Users |
12/11/2019 7:01 PM | |
Joined: 3/1/2019 Last visit: 4/2/2024 Posts: 17 Rating: (0) |
Hey, The Pin-Out using the cables from the "ethernet" wiring should change depending on the color standard you use (see image below and check your cables). Of course, the numbering doesn´t change, but please be aware of the colors you are using (in my case I use the A configuration). One thing I did not understand is: - Pin 1:White-Orange ???? -Pin 2: Orange ???? Shouldn't it be : - Pin 1:White-Yellow -Pin 2: Yellow (I'm thinking you are using the "B" configuration) So for me, in summary, should be: Profinet | Profinet Color | RJ45 number | RJ45 "A" color 1 | Yellow | 1 | White-Green 2 | Orange | 2 | Green 3 | White | 3 | White-Yellow 4 | Blue | 6 | Yellow |
Last edited by: RW_CPN at: 12/11/2019 19:03:09 |
|
This contribution was helpful to1 thankful Users |
Follow us on