12/11/2019 8:59 AM | |
Joined: 9/25/2019 Last visit: 4/20/2021 Posts: 21 Rating: (0) |
Hi, I have a problem - PH does not accept data from redundant servers (OS1, OS2). Previously, I reinstalled PH, migrated, and start PH with the OS servers. After that, PH changed its state from Active -> Active (Recovery) and on StandBy OS2 logs are created (attached). OS servers do not send data to the PH. The connection is established, there are message queues, the necessary services and processes are running: - Message Queue - Active (Start) - CCAPHServer - Active (Start) - Message Queue Connected. DIRECT = OS:PH\private$\PHlgRTData$=14 - Logging into PH-ready from the user account PH - OS servers are synchronized The settings were made according to the manuals: - Process Historian 2014 SP1. Process Historian - Administration - Installation and Commissioning of Process Historian and Information Server in a PCS 7 Environment - I read the post https://support.industry.siemens.com/tf/at/en/posts/problem-with-process-historian-no-tags-are-stored/147602?page=1&pageSize=10 Active (Recovery) on the PH has been going on for almost two weeks now (ProcessID 2324 - Recovery Sent/Recovery Started/Recovery completed) P.S. Prior to reinstalling the PH server on OS servers, the SFCache folder contained data. After reinstalling the PH, this data did not move to the PH. I can’t delete Cache from the servers, because I need the server to be up and running. P.S. I looked through similar topics on the forum, but the described actions did not bring results. Logs in the attach |
Last edited by: Pagle at: 12/11/2019 11:07:01 |
|
12/11/2019 9:01 AM | |
Joined: 9/25/2019 Last visit: 4/20/2021 Posts: 21 Rating: (0) |
2019-12-05 05:31:12.720: [Information] 2019-12-09 10:06:54.667: [Information] 2019-12-09 09:10:45.460: [Information] AttachmentOS1_OS2_PHSFSettings.txt (256 Downloads) |
Last edited by: Pagle at: 12/12/2019 06:59:36Last edited by: Pagle at: 12/12/2019 07:02:14Last edited by: Pagle at: 12/12/2019 07:03:07 |
|
Follow us on