12/14/2019 4:26 PM | |
Joined: 3/14/2008 Last visit: 5/6/2024 Posts: 2066 Rating: (928)
|
Hi, It could be numerous of things. For instance, if the picture tree was created in the OS project and not from the plant hierarchy. If you compile the OS and set option to generate picture tree from plant hierarchy, the settings can be lost. Or you may have read in a server package data from another server which is edited,removed. |
If I could help you, you can use the RATE button. Thank you. |
|
12/15/2019 4:26 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear FKSIEMENS, Could you check the OS Client project OS Project Editor? You may reassign the area again in the wincc explorer os project editor in ES. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
12/16/2019 3:07 PM | |
Joined: 8/12/2018 Last visit: 4/1/2024 Posts: 4 Rating: (0) |
dear all: thanks all your suggestions, I tested all yours methods, but not solve this issue! I did a simulation test use my laptop, just compile the project without any changing then download, no warnings and errors! Then I opened the os project editor, found in the os project editor area option, the hierarchy order is not correct! please see the attached! what's the reasons? AttachmentPCS7 overview area picture tree issue.pdf (84 Downloads) |
Follow us on