6/13/2023 7:58 AM | |
Joined: 1/17/2022 Last visit: 11/28/2023 Posts: 1 Rating: (0) |
I'm having the same issue, I try to type in "x2" it replaces it with the character "[". Did you find a solution? |
6/13/2023 9:23 AM | |
Joined: 1/21/2013 Last visit: 9/19/2024 Posts: 3119 Rating: (488)
|
Hi, PROFINET requires DNS compliant device names. However, even if the device name tried by Kiuas is DNS compliant, it does not match the naming rules used by Siemens. These rules do not allow the device name to start with a number. For details see section "Rules for the converted name" of "Assigning addresses and names to PROFINET devices". Kind regards |
Follow us on