10/10/2019 8:58 AM | |
Joined: 8/25/2006 Last visit: 9/19/2024 Posts: 2209 Rating: (278) |
Hello. Some time ago there was FAQ "How is STARTER manually uninstalled?", but now the link don't work. This FAQ was for Starter V4.4 in Windows7. I have attached description from this FAQ. You could try it, but use it at your own risk. Anyway I think it is better to reinstall all Siemens SW, may be reinstall Windows and Siemens SW. AttachmentManual_Uninstallation_STARTER_V4.4.txt (717 Downloads) |
This contribution was helpful to2 thankful Users |
12/19/2019 2:00 PM | |
Joined: 7/5/2009 Last visit: 6/27/2024 Posts: 76 Rating: (8) |
Hi For a complete manually uninstallation of STARTER Siemens recommend the following procedure: (1) uninstall STARTER via "Add/Remove Programs" control panel (2) go to the paths: Siemens\Step7\s7data\nsbmp Siemens\Step7\s7data\s7hdsc Siemens\Step7\s7data\s7htxt Siemens\Step7\s7data\s7hwprf\* Siemens\Step7\s7hlp Siemens\Step7\s7met and delete all u7* -files (3) go to the path Siemens\Step7\s7bin and delete the files: bi_cv_scripts.txt bi_drv*.txt bi_dv*.txt bi_go__drv.txt bi_to_*.txt bi_tp_*.txt bi_xquery.txt EditorTemplates.xml mkcfgdb*.bat ObjectModelInternal.tlb Siemens.MC.Starter.*.dll u7* umccfg.cfg umcInclude.manifest uninst_deviceom_* uninst_simotionom_* uninst_slaveom_* unregister.ssp_* (4) delete the paths: Siemens\Step7\u7umc Siemens\Step7\s7bin\u7setup (5) delete in the Registry under HKEY_LOCAL_MACHINE\Software\Siemens (32Bit) HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens (64Bit) the entry: DriveES (6) delete in the Registry under HKEY_LOCAL_MACHINE\Software\Siemens\AUTSW (32Bit) HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens\AUTSW (64Bit) the entry: STARTER (7) delete in the Registry under HKEY_LOCAL_MACHINE\Software\Siemens\Shared Components (32Bit) HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens\Shared Components (64Bit) the entry: UMC (8) delete in the Registry under HKEY_LOCAL_MACHINE\Software\Siemens\Shared Tools (32Bit) HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens\Shared Tools (64Bit) all entries: DCBLIB* DCC-Help System INFO SSP_* (9) delete in the Registry under HKEY_LOCAL_MACHINE\Software\Siemens\STEP7\2.0\Applications (32Bit) HKEY_LOCAL_MACHINE\Software\Wow6432Node\Siemens\STEP7\2.0\Applications (64Bit) the key: SIMOTION Attention! Use "delete shared component registry" (10) only if there are problems with shared components. (10) delete shared component registry: extract contents from the archive "Remove_Comp_STARTER_V5.3.zip" ( attached below )to a temporary directory execute "Remove_Comp_STARTER_V5.3.reg" by double click (11) reinstall STARTER AttachmentRemove_Comp_STARTER_V5.3.zip (535 Downloads) |
You can only go as far as you push |
|
This contribution was helpful to3 thankful Users |
Follow us on