12/19/2019 3:30 PM | |
Posts: 2 Rating: (0) |
Hello. I am new to step 7. I have a backup which I am not sure whether it is update but it has comments. I also tried to get an upload from the station to the PG but this upload had so many missing GSD files( because of the many different components on the profinet network(lenze drive, scalable switch etc) is there a way I can upload over the backup (may be just update the backup)that I have so that:-1- I get a backup I am sure has the comments and is update,2- so that I do not have to worry about the GSD files ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/20/2019 07:54:35New subject after splitting |
|
Follow us on