12/4/2019 3:18 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello emregns; Siemens S7-1200 PLCs use Profinet natively, so the easiest way to connect to a 3rd-party drive is through a Profinet interface on the equipment. Here are some Mitsubishi drives that advertise their Profinet connectivity: MR-J4-TM Servo (PROFINET®) Overview | Mitsubishi Electric ...Mitsubishi A8NPRT_2P Profinet Communications InterfaceMitsubishi Profinet 2 port Interface for FR-A/F800And here are some from Allen-Bradley : PowerFlex 20-750-PNET Profinet Single-port Option Module ...PowerFlex Low Voltage Drives Selection Guide - Literature ...There are also gateways from the drive Ethernet protocol to Profinet (Ethernet/IP for Allen-Bradley, for example). You can also look at Ethernet TCP/IP connections on the S7-1200, there are quite a few threads on the subject here on the forum: S7-1200 TCP communication – Sample program .So basically, it all depends on which drive you will choose and the communication capacities that the manufacturers have provided them with. Come back to us for more information when your decision has been made. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
12/25/2019 2:38 PM | |
Joined: 9/21/2012 Last visit: 4/26/2024 Posts: 3930 Rating: (444) |
You should be able to get examples and manuals from Rockwell, for your problem. |
Follow us on