12/28/2019 9:07 AM | |
Joined: 4/3/2019 Last visit: 10/19/2023 Posts: 6 Rating: (0) |
hi, dears i want to connect a device with a Modbus network to a Profibus network through a fiber optic cable. How can I do this object? ------------------------------------------------------------------------------------------ |
Last edited by: mpy65 at: 12/28/2019 10:40:27Last edited by: Jen_Moderator at: 12/30/2019 09:57:02New subject after splitting |
|
12/28/2019 12:16 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello mpy65; Extension of a Profibus-DP network over fiber optic cable requires OLM modules (optical link modules). If you look at the screenshot below, you might notice that each OLM has a Sub-D 9-pin connector (for connection of a standard copper Profibus segment) and fiber-optic connectors for the F.O. cable). So the OLM act as a network transition from copper to F.O. You can use plastic or glass cable with varying distances available, in linear, star or ring topologies. Details can be found in the OLM operating instructions manual: https://support.industry.siemens.com/cs/us/en/view/109476821 To insert a Modbus transition on the Profibus F.O. segment, the easiest would be to insert an ET 200_ station at the endpoint of the F.O. cable, with a Modbus master module in the final station. It is difficult at this time to propose definite equipment since you do not mention your PLC family or programming software, but ET 200M supports CP 341 as Modbus Masteror slave, ET 200SP supports the CM PTP as Modbus master or slave... that could all be used in such a network. Hope this helps, |
Last edited by: dchartier at: 12/28/2019 15:27:35Last edited by: dchartier at: 12/28/2019 15:28:45 |
|
This contribution was helpful to1 thankful Users |
Follow us on