Industry Online Support
Technical Forum
12/30/2019 5:50 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1423) |
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. As from the TIA V16, there was the introduction of the WinCC Unified. This is an engineering platform for HMI Comfort Unified and for WinCC Unified PC. It brings many news regarding the WinCC Advanced / WinCC Professional. One of the news of WinCC Unified is the support of Check box / Radio button. This sample project exemplify both elements. TIPs for Check box
TIPs for Radio Button
Project (.zap16 ziped as .zip) AttachmentProject6.zip (904 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
Follow us on