Industry Online Support
Technical Forum
12/30/2019 6:52 PM | |
Joined: 9/23/2005 Last visit: 9/17/2024 Posts: 4347 Rating: (1446) |
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Trends are an important tool for process signals evaluation. E.g. Trends are related to time, but there is situation where the trends should display the relationship between two variables. There is many variations about Function Trends, this example shows a simplest one. Configuration main steps:
TIP: To add more tags to the Trend Object, go to General → Trend Areas → [0] Trend Area → Trends; Click on 1 Object, "..." button, <Add new> TIP: To split the Trend Area in separet trends, go to General → Trend Areas; Click on 1 Object, "..." button, <Add new> To simulate values on the tag: drag and drop (select the tag on project tree, HMI tags, default tag table, details view windows) the HMI_Tag_1 / HMI_Tag_2 to the screen Project (.zap16 ziped as .zip)
AttachmentfuncttionTrend.zip (693 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
5/27/2024 10:27 AM | |
Joined: 9/23/2005 Last visit: 9/17/2024 Posts: 4347 Rating: (1446)
|
Hi, As from TIA V19 up2 it is possible to execute button function outside of the control by the ExecuteToolbarButton system function. More details see the post “Simple Sample and TIPs - WinCC Unified - execute button function outside of the control” at https://support.industry.siemens.com/forum/br/pt/posts/simple-sample-and-tips-wincc-unified-execute-button-function-outside-of-the-control/317497/?page=0&pageSize=10 |
Denilson Pegaia |
|
Follow us on