12/31/2019 2:25 PM | |
Joined: 2/1/2010 Last visit: 9/19/2024 Posts: 150 Rating: (71) |
Tekabi- Example: (example is complaint with domain integration and SIMATIC Logon groups created as another layer on top if needed) ES/OS/Clients all get the following local accounts and all passwords match on all machines: Administrator - Admin - only used for installing software/maintenance Since the SrvClient and SrvServer accounts are on both machines, file sharing is fine. Since SrvClient is a User type account, it is safe for your operators to not be able to mess with the machine too much if they can get past WinCC to the desktop. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to2 thankful Users |
Follow us on