1/5/2020 7:50 AM | |
Joined: 1/30/2018 Last visit: 7/23/2024 Posts: 18 Rating: (0) |
hello sir, i was using et-200 im151-8 pn/dp cpu and its was running with master plc 1200 and onother et-200 cpu of same type ,.all was ok and program were running good. but after some month. problem occure . here problem is that one of theET-200 IM151-8 PN/DPis gone in stop mode , and try to connect it to check diagnostic to find my problem.. but i was not able to connect it. i was unable to make it online error came wile doing online. connection failed or host not found, unable to connect. i ping the ip its was pinging .. but i can find my cpu while download during this another erroe occure 0132:000002 connection failed. some times after power reset its start loading but afer complile it show "connect host unreachable" possible thing i have tried.. like change ip address of my network and sharing connection. pg/pc set up network, interfarence network with subnet node , ip protocol, accessiable device, ** now i have change the cpu ET-200 IM151-8 PN/DP with same configration. still not able to connect . problem arise the same. now i have make new project and try to do online as when i do accessiable device, i found two device one is ip 192.168.0.1 and other is ios mac device. i tried to download with both device but not able to connect. again i thing is that problem may be the same .. here 1) Configuration- plc is- IM 151-8 PN/DP CPU - 6ES7 151-8AB01-0AB0 Interfacing module is- IM 151-3 PN-6ES7 151-8AB01-0AB0 Power module- PM-E DC 24V -6ES7 138-4CA01-0AA0 Expansion module- 6ES7131-4BF00-0AA0 2)Operating system is- Windows 7 3)TIA portal- TIA PORTAL V12 sp1 4)PG/PC- ETHERNET PORT i have studied all the discuss links but not help me out:- links 1. https://support.industry.siemens.com/tf/WW/en/posts/problem-in-downloding-a-program-to-im-151-8-pndp/116950?page=0&pageSize=10 error links 2. https://support.industry.siemens.com/tf//WW/en/posts/error-0132-000002-and-cpu-not-reachable/162728?page=0&pageSize=10 3. https://support.industry.siemens.com/tf//ww/en/posts/hmi-download-error-0132-0000002/167826?page=0&pageSize=10 4.https://support.industry.siemens.com/tf/ww/en/posts/want-to-communicate-s7-1200-and-s7-1500-by-profinet-to-share-io/223316/?page=0&pageSize=10 please help me to find out the problem.. where i am wrong ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/07/2020 06:08:58New subject after splitting sanjay63 |
|
1/6/2020 4:01 AM | |
Joined: 1/30/2018 Last visit: 7/23/2024 Posts: 18 Rating: (0) |
sir, sorry for twice but i i am not geting support that i want.. not any reply |
sanjay63 |
|
1/7/2020 6:10 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Jen_Moderator |
Follow us on