1/3/2020 7:23 AM | |
Joined: 9/20/2018 Last visit: 1/2/2024 Posts: 42 Rating: (4) |
Hello Everyone, I am also facing same issue . I am using PCS7 V9.0 SP2. I have 3 PC all 3 are dual screen. Out of 3 PC 1 PC is ESOS and remaining 2 Are WINCC Referance (OS). In Wincc Referance i can not able to access Interlock , Permission , Protect as well As jump. Interlock permission , protect are grayed out and Faceplate jump is not showing. Please refer attached PIC also. However In ESOS i can able to access everything. Both Wincc having same User. Also user given all the Permission. Please Help. Thank you in advance. ------------------------------------------------------------------------------------------ AttachmentSupporting_Screenshot.zip (104 Downloads) |
Last edited by: AutoGen_6024931 at: 01/03/2020 07:23:58Last edited by: Jen_Moderator at: 01/03/2020 09:07:42New subject after splitting |
|
This contribution was helpful to1 thankful Users |
1/7/2020 10:26 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Dear AutoGen, I faced this problem before. The issue might relate to server data. If you try to configure a server-client configuration / single OS configuration, it will work. Did you assign OS Server in your Client OS and download to the Target Station? Please also check these two links. Interlock button remains greyed out CEMAT V8.2 Faceplate Issue - Can't access Interlocks and Groups |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on