1/8/2020 6:31 AM | |
Joined: 11/16/2019 Last visit: 8/26/2024 Posts: 1 Rating: (0) |
Hi Friends, I am using the CPU414-5 H PN/DP and CP443 Module for Each Rack (Rack 0 and Rack 1) for the Redundancy Configuration. Actually I was configured the CPU and CP Ethernet IP Address using with Hardware MAC address. But after long back now i am unable to communicate with the CPU through IP Address (via CPU and CP Module IP Address). Event i couldn't ping the any one of the IP Address and MAC Address also. Presently temporally i am using MPI Cable for downloading and Monitoring the status. So, any one can support to solve the issue. Please give your suggestion's to solve the issue to proceed to my work. regards, M. Suresh Kumar ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 01/08/2020 09:44:44New subject after splitting |
|
Follow us on