1/9/2020 11:02 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi again, You have nice questions. I find the whole print editor in SFC a bit disappointing, because a print out can run through different sheets of paper. A print cannot be outlined in a nice manner. The print editor has become better in the past couple years, but I also have still problems with it. You can play with the print settings via SFC->Print and under column: Sequencer, you can select how to display the SFC: with properties, Normal size, Overview, with step transitions and under column: Options, you can select how alternative branches are aligned and comments. So I ques you have to play with it a little. What I normally do is print the whole SFC steps and with the Windows editor (Snipping tool Windows 7/10) I cut a few steps from the pdf and paste them in a word document so it has a better view. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to3 thankful Users |
Follow us on