Industry Online Support
Technical Forum
1/10/2020 6:52 AM | |
Joined: 8/27/2013 Last visit: 12/17/2023 Posts: 21 Rating: (0) |
Hello, I need to connect in PCS7 one PLC, which has a reserve Modbus TCP channel. WinCC as i understand did not allow double(reserved) Modbus TCP connections, so i want to use hardware device Modbus TCP <-> PROFInet produced by Phoenix Contact(FL RED 2003 E PRP)But I can't find any GSD files to insert it into NetPro. Does anybody used already this device and how i need to configure this connection? |
Follow us on