11/27/2018 3:36 PM | |
Joined: 10/9/2018 Last visit: 11/29/2023 Posts: 26 Rating: (0) |
Thank you very much! I appreciate the help! |
3/27/2019 2:54 PM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
Hi there, this statement is not correct ... the mentioned article number is a 3RW5 Soft Starter: It is part of SIRIUS Software "Soft Starter ES" (TIA-Portal): There exists also GSDML (PROFINET) and GSD (PROFIBUS) depending on the 3RW5 communication module type you are using: GSD file for SIRIUS 3RW52/3RW55 soft starter with PROFIBUS module GSDML file for SIRIUS 3RW52/3RW55 soft starter with PROFINET Standard module kind regards |
3/28/2019 6:59 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22230 Rating: (2980)
|
the GSD/GSDML is for the optional Communication Module! The 3RW5225-1TC04 itself have no fieldbus, but can be extended with the CP! |
9/26/2019 11:50 AM | |
Joined: 2/19/2015 Last visit: 7/3/2023 Posts: 3 Rating: (0) |
Hello, These GSD files are for steps7 v5.5 For TiaPortal V15.0 they don't work
|
9/26/2019 12:54 PM | |
Joined: 2/19/2015 Last visit: 7/3/2023 Posts: 3 Rating: (0) |
Sorry, it's all ok. Thanks |
1/13/2020 11:21 AM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
@ChristophD : That is why I did write "...There exists also GSDML (PROFINET) and GSD (PROFIBUS) depending on the 3RW5 communication module type you are using …" |
This contribution was helpful to1 thankful Users |
Follow us on