1/13/2020 1:11 PM | |
Posts: 1 Rating: (0) |
Hi all, i have plc siemens S7-1200 series.. I would like to conmect it to AB PowerFlex 755 through with profinet card. The modules name is 20-750-PNET Profinet single port I have downloaded the GSD File and install it to TIA Portal 15.1 But plc always getting error, plc cannot find the device eventhough i have make sure i can ping the profinet module Please help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/13/2020 13:26:55New subject after splitting |
|
This contribution was helpful to1 thankful Users |
10/6/2022 3:20 PM | |
Joined: 6/28/2016 Last visit: 12/7/2023 Posts: 4 Rating: (0) |
It has done?? It is possible to do this for PLCs from the eastern market (from China). |
Follow us on