1/9/2020 12:58 PM | |
Joined: 9/1/2017 Last visit: 11/22/2023 Posts: 3 Rating: (0) |
Dear Experts, I am trying to establish a connection between OPC and S7-1500 PLC with the help of PLCSIM Advance. I am getting data in OPC Scout with Bad_Timeout condition. Kindly find the attached document for the same. What can be done to avoid this kind of error? Kindly suggest. ------------------------------------------------------------------------------------------ AttachmentOPC Error1.pdf (110 Downloads) |
Last edited by: The Helping Hand at: 01/09/2020 14:23:12New subject after splitting |
|
1/14/2020 12:55 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735) |
Hello indalvit Why do you use this Solution instead of using the integrated OPC UA Server of the S71500. then you do not have to use SIMATIC NET OPC Server. If you have to use this solution then check this FAQ: https://support.industry.siemens.com/cs/ww/en/view/67295801 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on