1/13/2020 7:45 PM | |
Joined: 9/23/2011 Last visit: 4/22/2024 Posts: 44 Rating: (0) |
Good evening to all, I'm trying to access by standard OPC (without OPC UA) from OPC Scout V10 to S7-1500 following the S7-1200 manual OPC connection, but I can't connect to S7-1500. Is there some particolar configurations? I disabled the optimized block on DB I need to access on PLC and enabled GET/PUT on PLC. Thanks to all ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/14/2020 10:04:59New subject after splitting |
|
1/14/2020 1:53 PM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12835 Rating: (1639) |
Hello there are some essential Informatoins missing in your description. If I understand correctly you do NOT use the OPC UA Server in the S71500. You want to use an OPC Server (Which OPC Server??) that communicates with the S71500 with S7 Protocol. Like this FAQ for Simatic Net OPC Server: https://support.industry.siemens.com/cs/ww/en/view/67295801 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on