1/14/2020 2:01 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, An easier way: Go to Options in CFC or SFC editor and select: Chart Reference Data. Under View you can select the desired function: For example, Accesses in SFC types: In there you can see in which steps/transitions connections are being used. Play a bit to get familiar with it. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on