1/10/2020 2:32 AM | |
Posts: 57 Rating: (0) |
Dear All We are not able to set communication in our spare SCADA and PLC PC. Please guide us attached the existing system communication setting and Hardware details AttachmentCommunication Architechture.pdf (63 Downloads) |
1/14/2020 4:02 PM | |
Posts: 57 Rating: (0) |
Sir Details of PLC and SCADA software is as below PLC:SIMATIC Manager, STEL7, Version V5.5+SP4 SCADA Software: WinCC Runtime, V7.3.0.0 I do not having experience is communication protocols. i attached some details in PG/PC setting. In Physical connection CPU side Having Two LAN Cables which are coming in switch.ant at PC side single LAN cable is connection. Please guide how it is setting/ AttachmentCommunication Details.pdf (39 Downloads) |
1/14/2020 10:07 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Vishal; Your pdf documents show that you have a WinCC Runtime (RT) installation; you need a WinCCDevelopment/Runtilme license (RC) in order to create the connections and tags for communications with a PLC. I hope you have this license. You will find all the necessary information for connecting WinCC to your S7 PLCs over Ethernet in the following manual: WinCC v7.3: Communication https://support.industry.siemens.com/cs/us/en/view/102691766 The manual starts with a list of available channels, used to communicate with various brands of PLCs, or communicating with different protocols. The section you need is called "S7 Protocol Suite", which shows all the ways you can connect between WinCC and S7 PLCs such as you are using.; the channel of interest to you would be Industrial Ethernet . The following discussion may help you with some aspects of the connections over Industrial Ethernet: See also this video showing the setup of a S7-300 PLC with WinCC v7.2 using Industrial Ethernet. The WinCC configuration starts around timestamp 3:00 min. You will see how the Tag Management is used to select the channel (Industrial Ethernet), setup a connection , create tags (linked to PLC variables in the Step 7 program) and associate the tags to elements of screens created with the Graphic Designer. The video is narrated in Arabic and French but you should have no trouble following the sequence of necessary steps, especially if you follow the steps in the suggested manual in parallel with the video https://www.youtube.com/watch?v=SzyynMCfcSY Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/14/2020 22:09:32Last edited by: dchartier at: 01/14/2020 22:21:44 |
|
Follow us on