1/18/2020 5:16 AM | |
Joined: 8/19/2017 Last visit: 7/29/2024 Posts: 79 Rating: (3) |
Dear Georg Berghof I don't have any function started with "W". actually I want to work with this library before buying it (I did not installed the library yet), so I download a sample project From HERE and tried to see how it works. Block icons of IL for S7 doesn't work correctly. Does anyone has this library installed? If yes, send the functions source code here so I can create them manually. Thanks in advance |
Follow us on