1/9/2020 9:30 AM | |
Joined: 11/15/2015 Last visit: 5/3/2024 Posts: 178 Rating: (28) |
Dear hisham99kafafy Configure WINCC flexible runtime on your PC and connect it to the same project in simatic manager. Which means that you will add that to your project ( your project contains TP177 also). Your wincc flexible runtime also contains all pictures the same hmi. I hope that you get it Regards |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
1/16/2020 4:26 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645)
|
Hello hisham99kafafy Its not 100% clear what you want do do. Please describe your Usecase a little bit more detailed. -> If you need help in Loading the Panel you can look at: https://support.industry.siemens.com/cs/ww/en/view/23802404 https://support.industry.siemens.com/cs/ww/en/view/23800567 If you need help in Setting up the connection then: https://support.industry.siemens.com/cs/ww/en/view/24109937 https://support.industry.siemens.com/cs/ww/en/view/42918861 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on