1/17/2020 12:34 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hai arunvt1992, I couldn't predict what can be your issue by having this information. without having your backup it's difficult to go forward now. Usually in "WinnCC alarm control" if you mention the server name and Operator messages selection its is quit enough to get alarms in runtime. Ensure you are doing all these changes with sufficient user rights. And, I can give some pieces of information in this case. Please don't apply any filters in the initial time. First, ensure that you are getting alarms in the "WinCC alarm Control" window. Then, go for filter selections. There is one easy way. Already you are getting alarms in "@Alarmnew.pdl". So, You can call it directly in a picture window and apply your filter property in it. This case also will work. Please look at the Configuration property of "@Alarmnew.pdl". You may get some information on it. that was configured automatically by the PCS7 database for your actual project structure. |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
Follow us on