1/18/2020 11:34 AM | |
Joined: 1/18/2020 Last visit: 6/13/2023 Posts: 1 Rating: (0) |
Hello I used TiaPortal V14 Sp1 for TP1200 simatic HMI,and i wanted to change the time of supervision fault which giving incorrect time of occurance ------------------------------------------------------------------------------------------ |
Last edited by: Tariq1994 at: 01/18/2020 11:44:03Last edited by: Tariq1994 at: 01/18/2020 12:36:10Last edited by: Jen_Moderator at: 01/20/2020 11:07:18New subject after splitting |
|
1/20/2020 3:29 PM | |
Joined: 8/3/2009 Last visit: 9/25/2024 Posts: 13788 Rating: (1741)
|
Hello you are talking about Supervision Fault,; are you talking about PLC Alarms like PLC Diagnostic alarms or Program_alarm or ProDiag Alarms? If yes then the Timestamp will be defined in the PLC. So the HMI Systemtime has to be the same as in the PLC.-> Do a Time Synchronisation! And you have to look also after the Localtime. The Timestamp comes with Systemtime of the PLc then you have to care about loclal time on the HMI. Here are the two important FAQs: https://support.industry.siemens.com/cs/ww/en/view/69864408 https://support.industry.siemens.com/cs/de/en/view/109482675 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on