1/15/2020 5:30 PM | |
Joined: 12/27/2018 Last visit: 7/17/2023 Posts: 509 Rating: (41) |
Additional Information :TIA selection Tool |
Jinson James, P.Eng, BE, M.Tech (Power System),PGDM, MBA |
|
This contribution was helpful to1 thankful Users |
1/17/2020 8:17 PM | |
Joined: 12/27/2018 Last visit: 7/17/2023 Posts: 509 Rating: (41) |
I have an opinion: Wireless is new revolution automation. You can use Siemens router to connect Remote stations via wifi to control room for non-critical system monitoring purpose. These kind of powerful wifi routers are used in mining industry for connecting Siemens Mobile(Wireless HMI) panel. Is the stations located far away then wifi signal need to be transferred like Substation Automation System to main control station. Then all about HMI design. I recommend use TIA Portal V16 WinCC unified for HMI design because this got many new features, for example, you can add a small screen in a big screen. Also use Siemens Sm@rt Clent facility via HTML server(refer the below video full length which shows example) and web server for monitoring remote PLC. Sm@rt client help to monitor and control remote HMI from control station. This need to be properly designed in Control room SCADA computer. Licenses:For example, one S7 1500 PLC and 10 comfort HMI You need licenses for TIA Portal V16 (Engineering /programming software) For Comfort panel does not need licenses unless any add-on.License list find in this link. Estimation & Selection: You can get prices and availability of material in Siemens stock by SIEMENS mall. For selecting material, I recommend just make a network architecture in TIA portal and check the material via Siemens selection tool. For more help, Siemens Can arrange regional sales representative for consultation who can help you to select most economical materials for your project budget. Which is your region? For any help for coordination with sales, you can talk to Moderator. Ask if you have any questions. |
Jinson James, P.Eng, BE, M.Tech (Power System),PGDM, MBA |
|
This contribution was helpful to1 thankful Users |
Follow us on