1/16/2020 4:15 PM | |
Posts: 5 Rating: (0) |
thank you dchartier.is there way for direct communication wincc v7 to sinamics120 without opc server? |
Last edited by: aramfe at: 01/16/2020 16:16:38 |
|
1/16/2020 10:34 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello aranfe; As per DJ_1's post ,entionned earlier: "As per my knowledge SINAMIC S120 having data block structure like S7 PLC, so this drive can directly operate via WinCC or HMI via S7300/400 channel". This I presume points to the Profibus or Profinet channel of the S7 Protocol suite, in WinCC v7.x. I have no further details personally, but the usual way to establich connunications through the S7 protocol suite involves setting up connections to a Profibus/Profinet partner, and creating tags that permit exchanging data between WinCC and the partner.. I believe this section of the Communication manual for S120 drives is the basis for DJ_1's comment. It is dedicated to Protool and WinCC Flexible, and there is no library for WinCC v7.x to control dietly a S120. But the information shown in the screenshot below may provide some hints for your application. SINAMICS S120 Function Manual Communication https://support.industry.siemens.com/cs/us/en/view/109771803 Hope this helps, Daniel Chartier |
1/20/2020 2:17 PM | |
Posts: 5 Rating: (0) |
we have plc s400.but i want to directly access without plc.i did with wincc flexible and wincc tia but i can't do with wincc explorer. |
Follow us on