Industry Online Support
Technical Forum
1/21/2020 4:00 PM | |
Posts: 2 Rating: (0) |
dear everyone I'm working with "TIA 15" and I want to control a shaft position with "PTO (mode : A /B phase_shifted)" but there is a problem ...! I've set all inputs & outputs & parameters correctly but the problem is although I see the speed & position changing in program , I'm not able to see the pulse train in the output ! In one word I have one pulse as moving the shaft in program & after I stop it , it turns to zero instead of being a pulse train . what should I do ? Thank all of you read and help me . P.S : I've attached my settings below [snip] AttachmentScreenshots.zip (39 Downloads) |
Last edited by: Jen_Moderator at: 01/22/2020 11:20:41Removed links and added files as an attachment. |
|
Follow us on