4/5/2016 1:14 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello, this sounds bad. Do you have an older version, an archived version or some other manual backup? Don't get your hopes up to high, but you can try the solution in this FAQ. Maybe the technical support can help you, when you send them the project file and the backup file (see lower part of the FAQ):
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/5/2016 3:02 PM | |
Posts: 6 Rating: (0) |
Thanks H.J. for the reply. I have a manual back up before one week and may be I will redo it. That is easier than to get in contact with tech support. Just wondering, Is there some software or method by which we can automatically have a backup for the TIA portal project !? or, is manual backup the only option ? |
4/5/2016 6:27 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
There might be a possibility using TIA openness. I think you could write a program it to save a backup project or to archive the project every night. You can find the available functions and demo projects here:
You need Microsoft Visual Studio and some knowledge on coding. |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
12/13/2016 3:37 AM | |
Posts: 1 Rating: (0) |
Hallo, Is the problem has been solved? I get same problem, |
1/22/2020 10:41 AM | |
Joined: 7/13/2011 Last visit: 3/25/2024 Posts: 3 Rating: (0) |
In V13 delete all files in the Logs folder except .ico You can then open the project. |
Follow us on