1/23/2020 10:51 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I need to add an alarm to my WinCC 7.4 Upd.1. I have made DA #30 in Tag Management and set it up like the existing 29 alarms. When I move to Alarm Logging I can also add DA #30 it is not accepted when I try to use the same signal (Ack_Alarm) as has been used on DA #3 - DA #29. And I wonder if the acknowledgement tag actually works on these alarms since the all have bit 0 chosen and this is shown as red. If I look at "Alarm_Kvitt" I CAN use bit 2 but where is the this bit controlled from (what is making it go high)? As additional question - where / how can I find where UDT102 is used? I would like to see where +0.6 Alarm_Kvitt is written and read for this UDT. What is the best way to set up alarm acknowledgement AttachmentOMS ALTXT.zip (88 Downloads) |
Follow us on