1/24/2020 8:11 AM | |
Posts: 3 Rating: (0) |
i am using pymodbus libary to read holding registers from el lg+1119 now i want to read total watt whose register address is 40101 data type is float code : from pymodbus.client.sync import ModbusSerialClient as ModbusClient
atmel_usart_serial atmel_usart_serial.0.auto: using dma0chan7 for rx DMA transfs ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/24/2020 11:46:33New subject after splitting |
|
1/24/2020 8:59 AM | |
Joined: 2/10/2012 Last visit: 9/18/2024 Posts: 314 Rating: (59) |
You write the only main difference is the processor... next version will also use debian but: https://en.wikipedia.org/wiki/Intel_Quark "Intel Quark SoC X1000 contains a bug #71538[12]that "under specific circumstances" results in a type of crash known as asegfault." This withheld me to try an iot1020. But this is not an issue when running yocto? And if you want to run Debian you should use the 1040? thx |
Last edited by: enof at: 01/24/2020 09:03:54 |
|
2/3/2020 6:13 AM | |
Posts: 3 Rating: (0) |
now for me it is getting values can i know how to send it thingsboard can u provide any source code pls using mqqt or http protocol . |
2/3/2020 2:14 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I'm not familiar with Thingsboard, but looking at the integrations guide I'm actually unsure if you can access them over the regular 1883 port as you are doing in your application. Kind regards! |
4/2/2021 4:21 PM | |
Posts: 1 Rating: (0) |
How you solve the error can u explain me |
Follow us on