1/28/2020 5:10 AM | |
Posts: 33 Rating: (0) |
I have digital inputs under 5V signal. Which PLC can read digital inputs ranging under 5v? |
2/3/2020 6:45 AM | |
Joined: 10/25/2019 Last visit: 2/28/2024 Posts: 276 Rating: (20) |
this wonder, gets TTL-levels (what you need) and outputs 24VDC. as concerned MOSFETs, the transistor itself isn't sole element on PCB. You will have to make PCB, envisage safety circuit, connectors, indication, housing, soldering, etc. Keep in mind. It's lucrative business when you need at least hundreds and more. If you need a few dozen. Forget. Better buy it, the link above. BR |
Last edited by: HBCM_ at: 02/03/2020 07:02:01 |
|
This contribution was helpful to1 thankful Users |
Follow us on