1/30/2020 10:30 PM | ||
Joined: 11/20/2011 Last visit: 3/29/2023 Posts: 80 Rating: (0) |
Dear, I am installing PCS7 v8.2. My drive C has not space, and I want to install the PCS7 in another drive like drive E. for PCS7 v8.1, there is a tpoic in : https://support.industry.siemens.com/tf//WW/en/posts/pcs-7-installation/159273?page=0&pageSize=10 However, the solution does not work for V8.2. There is not
in the setups.ini file. I need to change the target directory, but it is not possible in the installation procedure. |
|
1/31/2020 5:51 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979) |
Hi, do you have some other SIEMENS Simatic SW installed? Christoph |
Follow us on