1/30/2020 2:33 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, It's sounds like you have not installed the Basic Library V7.1 SP3. This library can be installed from the media DVD of PCS7. This is the classic library which is discontinued. You can still use the library, but you have to install it. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/30/2020 2:52 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Can you check the DVD under additional tools. It should be there somewhere |
If I could help you, you can use the RATE button. Thank you. |
|
1/31/2020 9:09 AM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating: (31) |
Hello together, let me help you. Here you can find the Library 7.1 SP 3 Upd4 https://support.industry.siemens.com/cs/de/de/view/109757344 Regards |
Last edited by: Technodrome at: 10/29/2020 22:51:37Last edited by: Technodrome at: 10/29/2020 22:53:47 |
|
This contribution was helpful to1 thankful Users |
Follow us on