2/4/2020 9:38 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
OK..So, Updating the reference and counter values in HSC database inside an interrupt does not speed things up at all as the counter will be updated only when the counter instruction is executed; you had that place in a cyclic interrupt and accordingly the counter values would be updated when the cyclic interrupt executes. It would make more sense to call HSC instruction in the hardware interrupt itself if the intention is to speed things up. AttachmentHSC_Forums2_1.zip (247 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on