6/8/2011 5:06 AM | |
Posts: 291 Rating: (68) |
HiSaravana,
No problem! It's my fault that I hadn't described it very clearly! (Forgive my poor English, please!) Sorry~ I'm not recommending of using "AutoStart" option. To be brief ~ typing "MSINFO32" is convenient for us to check what a "Formal Commandline with Parameters" WinCC calls for starting the Runtime is. & we may copy & paste the Commandline for using directly for a "ShortCut Command" or for a "Shell Execution" & so on writing as: "C:\Program Files\Siemens\WinCC\bin\AutoStartRT.exe D:\1_Project\Audio_MuteSwitch\Audio_MuteSwitch.MCP /Activ:yes /LANG=ENU /EnableBreak:yes" 1. AS you may know the parameterfor setting RT-Language is "/LANG=ENU" for example. 2.Parameterfor start runtime is "/Activ:yes". 3. You may also set the parametercontaining path for a redundant server (with project). 4. & you know already ~ executing of this command line won't bring you the WinCCExplorer window. So...I was talking about a way toCapturecommand & paramenters quickly. This method can be implemented for other "Application"... as you may see the "C:\Program Files\Siemens\SimaticLogon\sldatabasehandlerx.exe" & something else wirtten already. *** & You may remove the "AutoStart"mechanism there by deleting the registered "Key" under [HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Run] No~ back to our discussion: Because you've given a right & good answer for everyone, so ~ I just simply wanted to give additional informtion for reference. I'm just too lazy to taking a note for execution command/services of WinCC or other program. So "msinfo32" is a good way for me. By the way, you've said you don't want the PDLRT executed (opened) in WinCC Runtime. If so ~ please do the configuration as the attachment. then, After calling your commandline (pressing your shortcut icon), RT will be activated without opening the HMI RT (PDLRT.exe.) Best regards, Komi P.S: There's also another VBS(WMI) method & so on... if you want! AttachmentRT_ServiceMode.zip (802 Downloads) |
Last edited by: Komi at: 6/8/2011 7:50 AM |
|
5/7/2013 8:52 AM | |
Posts: 65 Rating: (1) |
Thank you Mr.Saravana Kumar for the Autostart Option. It is good to use. Regards, Raghu
|
2/5/2020 10:58 AM | |
Posts: 1 Rating: (0) |
its not working in wincc 7.4 sp1 |
Follow us on