2/6/2020 9:01 AM | |
Posts: 87 Rating: (0) |
Hello to All, I am using Simotion D445-2 DP/PN, 6AU1 445-2AD00-0AA0, version V5.3, sinamics version V5.2. Simotion goes to Stop state every few days and i am not sure what is the reason. I am missing licences for CAM, GEAR and Extended Safety Integrated, so can be that the reason? It says " Message bufer overflow with technological alarms", " Stop caused by technological alarms", "One or more runtime software licences missing"..etc... Please find attached Simotion Diagnostic. Just for the help, last transition to STOP mode was today at 6:41AM. (6.2.2020). Thank you in advance. Best Regards, AttachmentDevice Diagnostics_3.txt (115 Downloads) |
2/6/2020 9:45 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
yes this can be the reason! you should elimeinat the fault cause for the 40202! |
2/6/2020 10:46 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, try the 3rd remedy , use higher synclength or reduce the master velocity regards christoph |
2/6/2020 11:57 AM | |
Posts: 87 Rating: (0) |
Hi, Please find attached some more info. Wheni record actaul accelaration, SetAcc is around 1200 and actual is around 25000. I increased Limits to 36000, but still the same fault.
Attachmentslave.zip (117 Downloads) |
Last edited by: manningcub at: 02/06/2020 11:58:26 |
|
Follow us on